High-quality instrumentation for cooling water systems
OEM Torishima benefits from reliable products and local service of Endress+Hauser
Torishima, an engineering solutions provider and original equipment manufacturer, needs reliable and high-quality instrumentation for its cooling water systems that it supplies to municipal water customers in the Middle East. The Glasgow-based company sources all of its instrumentation for the skids, including temperature sensors, pressure transmitters and flowmeters, from Endress+Hauser and has praised the reliability and performance of the products, as well as the customer service.
The result
Remote access to instrumentation from the control room – essential in high-temperature environments
High-performing instruments with excellent quality and durability for reliable operation over decades in demanding conditions – fewer breakdowns meaning safe water supply for local communities and fewer service visits to the customer
On-time delivery of devices to the customer
Reliable and local customer service for quick support on site in the case of problems
The customer requirement
Cooling water systems are essential to ensure the safe, efficient and reliable operation of pumps and other equipment, as overheating can damage components, affect performance and compromise the overall stability and reliability of the pumping station. “These systems have to operate for 25 to 30 years, and breakdowns can be a major problem,” explains Projects and Operations Director Tom Coutts.
Our solution
Endress+Hauser supplies temperature sensors, pressure transmitters, point level switches, flowmeters and flow switches for the skids, all of which can be accessed remotely from the control room. In such demanding conditions, the quality and durability of the instrumentation is important. “Everything has to be stainless steel and to the strict specifications of the end user,” explains Tom Coutts. “If a cooling system goes down, it has a huge effect on the local community. Sending a service engineer from Glasgow to the Middle East is very expensive, so I need reliable equipment.”
Devices used
Proline Promag W 10 electromagnetic flowmeter for accurate measurement of cooling water even after bends in the tube thanks to 0 x DN full-bore option
iTHERM ModuLine TM131 intrinsically safe temperature sensor