키워드, 주문 또는 제품 코드 또는 일련 번호를 검색해 보십시오(예: “CM442” 또는 “기술 정보”).
검색하려면 최소 2자 이상 입력하십시오.

Preheater & cyclone optimization: Eliminating blockages and heat loss

Process behavior, measurement limits and control requirements for stable preheater and cyclone optimization.

Cement plant preheater tower with multiple cyclone stages for heat transfer and material separation
Introduction

Beyond blockage prevention: The strategic value of preheater optimization

The preheater tower and its cyclone stages contribute more than half of the thermal efficiency of a modern cement plant. As the main heat‑recovery and separation system, the preheater determines how effectively the entire pyroprocess operates. Its performance depends on two fundamentals: consistent heat transfer and stable material flow.

It requires constantly managing blockages, buildup and false air. Even small deviations in the preheater’s behavior can increase fuel consumption, disturb kiln stability and impact clinker quality.

Preheater optimization targets these sources of variability, transforming the preheater into a stable and predictable part of the process. With reliable measurement data, operators can detect early signs of flow restrictions, air leaks or thermal imbalance, intervene before issues escalate and keep the kiln supplied with consistently conditioned feed.

Cyclone preheater process diagram ©Endress+Hauser
Cyclone preheater process diagram

Cyclone preheater

Insights

Preheater process overview in cement production

The preheater transfers heat from the kiln exhaust gases into the descending raw meal and separates solids from the gas stream across multiple cyclone stages. Each stage raises the meal temperature and improves calcination efficiency before it enters the kiln inlet.  

Stable operation depends on controlled gas velocity through the riser ducts, consistent meal flow through the dip tubes and balanced draft across all cyclone stages. When these conditions hold, the system delivers predictable thermal loading and separation behavior to support stable kiln operation.

Cement plant preheater tower with cyclone stages for heat transfer in clinker production ©Adobe Stock/romannoru
Insights

What causes preheater instability in cyclone towers

Several factors can disrupt stable preheater and cyclone operation. These disturbances typically arise from changes in fuel behavior, gas composition or material‑flow conditions. The interaction between rising hot gases and descending meal is highly sensitive; even small shifts can affect separation accuracy or draft balance. Because conditions in each cyclone depend on those in the previous one, local deviations often propagate through the entire tower.

Typical disturbance mechanisms are:

  • Fuel variability: Alternative fuels and high‑sulfur petcoke alter combustion temperatures and volatile content, increasing the likelihood of sticky material and buildup formation in risers and cyclones
  • Temperature and gas‑composition changes: Deviations in temperature profiles or elevated sulfur or chlorine-related cycles influence gas density and dust loading, reducing separation quality
  • Restrictions at the kiln inlet or within cyclone stages: Reduced cross‑section increases pressure loss, disturbs draft distribution and forces the Induced Draft (ID) fan to compensate. Meal accumulation in dip tubes or risers accelerates deposition and raises local temperatures
  • Cyclone blockages, ring formation and corrosion: Excess dust circulation, volatile cycles or temperature extremes can create progressive restrictions
  • Frequent kiln stops for cleaning: Severe buildup eventually requires manual removal, causing downtime and thermal stress on equipment

Over time, these factors make it difficult to maintain consistent cyclone performance and thermal balance. This reinforces the need for robust measurement and reliable gas‑analysis data to detect early signs of draft shifts, buildup tendencies or combustion deviations.

Cement plant with preheater tower, silos and processing units in clinker production ©shutterstock/B Brown
Insights

Measurement challenges in harsh preheater environments

Measuring reliable data in the preheater tower is difficult due to several harsh environmental conditions.

Key stress factors:

  • Extreme dust loading: Rapidly clogs temperature, flow, O₂ and dust measurement paths. Without the right technology for dusty applications, sensors can drift, blind or deliver unstable signals
  • Erosive, hot and chemically aggressive gas streams: Wear down exposed sensor surfaces and housings, especially in riser ducts and high velocity cyclone areas
  • Thermal cycling and condensation: Repeated heating and cooling cause corrosion, moisture ingress and blocked sampling lines
  • Limited accessibility: Many measuring points are difficult to reach, so any cleaning, purging or calibration strategy must be engineered for long intervals. This is a key concern for maintenance, quality and operations teams

Since these factors degrade instruments over time, maintaining data quality is a continuous challenge.

Cement preheater towers with cyclone stages and ducts in clinker production plant ©Endress+Hauser
Insights

Key measurements for preheater cyclone optimization

Accurate measurement in the preheater tower requires instrumentation that can tolerate dust, abrasion, thermal shock and chemically aggressive gases. Only robust, contamination‑resistant technologies maintain stable signals under these conditions. When data remains drift‑free, operators can detect deviations early enough to prevent restrictions from developing into full blockages.

  • Temperature: Temperature profile across cyclones and risers. It reveals gas–meal balance, separation efficiency, hot‑spot formation and early buildup tendencies
  • Pressure: Stage pressure and differential‑pressure trends across cyclones and strings. Primary indicators of dust loading, rising flow resistance and emerging blockages
  • Level: Non-contact buildup or blockage detection in dip tubes or risers. Radiometric, microwave or radar methods are used where mechanical sensors cannot survive due to abrasion, temperature or buildup. They detect material accumulation before it affects gas flow
  • Dust loading: Inferred from ΔP rise, temperature deviations or optical attenuation signals. Direct dust measurement inside the tower is rarely reliable because fouling quickly blinds sensors. Instead, the combination of ΔP trends, temperature anomalies and optical path attenuation acts as a practical proxy
  • Process gas conditions: Gas behavior at the kiln inlet, calciner and preheater outlet. Operators interpret these primarily through stable temperature and pressure patterns, because direct in‑situ gas analysis inside the riser is nearly impossible due to fouling and high dust burdens
  • Process gas composition: Key combustion and cycle related gases in the preheater. These are monitored as process measurements rather than environmental stack emissions

Collectively, these measurements give operators a clear picture of draft balance, material flow and combustion behavior inside the tower. When the signals remain stable and timely, deviations can be detected early, allowing intervention before blockages, buildup or heat‑transfer losses escalate.

Cement plant with preheater tower and process units for clinker production ©Adobe Stock/bilanol
Insights

How reliable measurements improve preheater optimization

When temperature, pressure, level and gas conditions are measured reliably throughout the preheater, the entire tower becomes far easier to stabilize. This enables the following improvements:

  • Higher cyclone efficiency and steadier kiln feed flow, thanks to early detection of rising ΔP, gas maldistribution and buildup formation
  • Lower heat consumption, as stable temperature profiles improve gas–meal heat transfer and minimize losses caused by false air or restricted stages
  • Fewer blockages and emergency shutdowns, with accurate measurement signals allowing operators to intervene before hydraulic instabilities escalate
  • Reduced maintenance exposure, as fewer build-ups mean fewer confined space entries, less refractory stress and lower mechanical wear on fans and ducts
  • More predictable ID fan and calciner operation, supported by stable O₂/CO/SO₂ behavior at the kiln inlet and calciner
  • Higher measurement reliability in dust-laden, abrasive and high temperature zones, reducing nuisance alarms and manual checks

Stable preheater operation ultimately depends on the integrity of the core measurements that define hydraulic and thermal behavior. When operators can trust the signals feeding their control loops, they can keep the tower within a narrow window instead of constantly reacting to disturbances. In an environment where dust load, abrasion and volatile cycles work against instrumentation, maintaining measurement robustness becomes a decisive factor for energy efficiency, output stability and long-term asset health.

FAQ

Frequently asked questions on preheater optimization

The following questions address common challenges in optimizing cyclone and preheater operation, from measurement reliability to early detection of buildup and flow restrictions.

문의 주시는 내용에 대해 최대한 상세하게 기재해 주시면, 보다 빠르고 정확한 응대가 가능합니다.

미주

Find out more