Title

키워드, 주문 또는 제품 코드 또는 일련 번호를 검색해 보십시오(예: “CM442” 또는 “기술 정보”).
검색하려면 최소 2자 이상 입력하십시오.

Efficient sludge treatment and process control in real time

Reliable measurement of total solids for wastewater treatment plant Bändlegrund with Proline Teqwave MW 500

Due to increasing legal requirements, wastewater treatment plants are continuously required to review their processes and optimize them, if necessary. In this context, operators of the Bändlegrund wastewater treatment plant in Weil am Rhein, Germany saw potential for optimization in sludge management. The installation of the Proline Teqwave MW 500 in-line measuring device from Endress+Hauser made it possible to optimize multiple areas at the same time.

Picture of Bändlegrund wastewater treatment plant in Weil am Rhein, Germany ©Endress+Hauser

Bändlegrund wastewater treatment plant in Weil am Rhein, Germany, has existed since 1983 and currently has a capacity of 290,000 PE.

Picture of Proline Teqwave MW 500 measures the total solids in sewage sludge at Bändlegrund ©Endress+Hauser

Proline Teqwave MW 500 measures the total solids in sewage sludge in real time using microwave transmission.

The result

  • Increased operational safety thanks to process stabilization

  • Reduced energy and polymer consumption due to optimized sludge treatment

  • Process control in real time

  • Minimized manual effort and optimized pump runtime performance

  • Increased digester gas yield

Steffen Mehlhorn, 
Managing Director of the Wieseverband 
wastewater association

"For us, it was very important that we optimize process control in sludge management in light of the increasing legal requirements in operation. We achieved this thanks to Teqwave MW 500."

Steffen Mehlhorn, Managing Director
Wieseverband wastewater association

The customer requirement

One optimization approach was the removal of primary and secondary sludge from the hoppers of the primary clarifiers. This process was controlled by the runtime of the sludge removal pumps. Adjusting the runtime required the results of a manual sludge level measurement and experienced personnel. Another challenge is the solids-based polymer dosing when dewatering the slurries. The solid content was determined manually and the amount of polymer was added in proportion to volume.

Our solution

Teqwave MW 500 is an in-line measuring device that displays the total solids in sewage sludge in %TS in real time using microwave transmission. Thanks to direct measurement in the inlet to the thickener, the flow of sludge can be balanced and pump runtimes can be automated. During sludge dewatering, real-time solids measurement enables the amount of polymer to be dosed in the inlet of the chamber filter press optimally at all times, even in case of changes to the solids content.

문의처

저희 제품에 관심이 있으십니까? 해당 작업 용도에 대해 상담받고 싶은신가요?

문의 주시는 내용에 대해 최대한 상세하게 기재해 주시면, 보다 빠르고 정확한 응대가 가능합니다.

  • 단순 제품

  • 손쉬운 선택, 설치 및 작동

기술적 우수성

단순성

  • 기본 제품

  • 신뢰성, 내구성, 유지보수가 쉬움

기술적 우수성

단순성

  • 하이엔드 제품

  • 우수한 기능성과 편리성

기술적 우수성

단순성

  • 전문 제품

  • 까다로운 어플리케이션을 위한 설계

기술적 우수성

단순성

구성에 따라 다름

FLEX 선택 기술적 우수성 단순성
  • F
  • L
  • E
  • X

Fundamental 선택

기본적인 측정 요구사항 충족

기술적 우수성
단순성
  • F
  • L
  • E
  • X

Lean 선택

핵심 프로세스를 손쉽게 처리

기술적 우수성
단순성
  • F
  • L
  • E
  • X

Extended 선택

혁신적인 기술로 프로세스 최적화

기술적 우수성
단순성
  • F
  • L
  • E
  • X

Xpert 선택

가장 까다로운 어플리케이션 요구사항 충족

기술적 우수성
단순성

구성에 따라 다름