Title

키워드, 주문 또는 제품 코드 또는 일련 번호를 검색해 보십시오(예: “CM442” 또는 “기술 정보”).
검색하려면 최소 2자 이상 입력하십시오.

Unbeatable alliance: tradition and progress!

Sustainable wastewater treatment during potato processing

Wernsing Feinkost GmbH places high value on the efficient and sustainable utilization of all resources. Wastewater is monitored, cleaned and filtered using advanced methods at the company’s own disposal and treatment center. 20 percent can be reused for the cleaning and processing steps, a rate that continues to increase. Endress+Hauser helps Wernsing execute its demanding sustainability strategy by providing the measurement and automation technology.

Proline Promag P flowmeter for demanding applications in wastewater treatment ©Endress+Hauser

Proline Promag P electromagnetic flowmeter for demanding applications in the wastewater treatment

Complete monitoring of the activation tanks with all kind of liquid analyzers ©Endress+Hauser

Complete monitoring of the activation tanks: ammonium and phosphate analyzers, as well as UV photometric measurement of nitrate with sample preparation.

Results

  • Reliable instrumentation from Endress+Hauser ensures optimal wastewater cleaning during all treatment steps, even with fluctuating amounts and concentrations of wastewater.

  • The excellent collaboration between the industry experts at Wernsing and Endress+Hauser continuously leads to new process improvements that further optimize efficiency and sustainability.

Dipl.-Ing. Wilfried Elberfeld, Wernsing Feinkost GmbH

“With Endress+Hauser we found a reliable partner who charts new courses with us and helps us implement our demanding sustainability goals.”

Dipl.-Ing. Wilfried Elberfeld
Disposal and treatment center, Wernsing Feinkost GmbH, Germany

Customer challenge

The Wernsing Food Family processes round 500,000 tons of potatoes each year, a significant share at the Addrup/Essen location in Oldenburg, Germany. Vast amounts of wastewater accumulate while cleaning and processing the potatoes. Wernsing reuses as much of the wastewater as possible as process water. The rest has to be discharged into the environment and sewage system in compliance with all regulatory restrictions.

Realization

The wastewater solids are filtered at the plant. All oils and fats are removed after an initial mixing and balancing step. Floating matter is removed during preliminary treatment. A second mixing and balancing step is used to standardize the pH value and temperature, which is then followed by anaerobic pretreatment of the wastewater. 80 percent of the contaminants is broken down here; the rest is removed during the activation and secondary treatment steps.

문의처

저희 제품에 관심이 있으십니까? 해당 작업 용도에 대해 상담받고 싶은신가요?

문의 주시는 내용에 대해 최대한 상세하게 기재해 주시면, 보다 빠르고 정확한 응대가 가능합니다.