키워드, 주문 또는 제품 코드 또는 일련 번호를 검색해 보십시오(예: “CM442” 또는 “기술 정보”).
검색하려면 최소 2자 이상 입력하십시오.

Self-calibrating thermometers in hygienic processes

Theory and practice

self-calibrating thermometer in a hygienic process ©Endress+Hauser

This white paper explains how self-calibrating thermometers can be used in hygienic process engineering. It details theory and practice as well as application examples.

How self-calibration works

The self-calibration method uses the Curie temperature (Tc) of a reference material as a built-in temperature reference. Self-calibration is performed automatically when the process temperature (Tp) drops below the nominal Curie temperature (Tc) of the device.

The electronics unit detects this change automatically and simultaneously calculates the deviation of the measured Pt100 temperature from the known Curie temperature, which is a physical fixed point.

문의처

저희 제품에 관심이 있으십니까? 해당 작업 용도에 대해 상담받고 싶은신가요?

문의 주시는 내용에 대해 최대한 상세하게 기재해 주시면, 보다 빠르고 정확한 응대가 가능합니다.