Title

키워드, 주문 또는 제품 코드 또는 일련 번호를 검색해 보십시오(예: “CM442” 또는 “기술 정보”).
검색하려면 최소 2자 이상 입력하십시오.

TECOSOL achieves stable biodiesel production with robust instrumentation

Reliable measurement technology stabilizes processes under variable operating conditions

산업: 화학
Biodiesel production process: stable operation with integrated measurement technology

문의 주시는 내용에 대해 최대한 상세하게 기재해 주시면, 보다 빠르고 정확한 응대가 가능합니다.

요약

TECOSOL is one of the leading biofuels manufacturers in Europe. They operate 2 plants and produce biofuel that achieves significant CO₂ savings compared to fossil diesel. Highly contaminated residues and waste materials, fluctuating feedstock compositions, high temperatures and vacuum conditions place demanding requirements on biodiesel production processes and instrumentation. Using the complete product portfolio from Endress+Hauser, TECOSOL GmbH operates a highly automated plant in Wittenberge that ensures cost-efficient, safe and stable production.

Ralf Türck, managing director of Tecosol

“With biodiesel from the new plant in Wittenberge, TECOSOL achieves over 90% CO₂ savings compared to fossil diesel. It represents one of the few effective solutions for decarbonization."

Ralf Türck, Managing Director, TECOSOL GmbH

The challenge: biodiesel production under feedstock variability and demanding process conditions

TECOSOL GmbH produces biodiesel from contaminated residues and waste materials generated, for example, in the timber industry and oleochemistry. The composition of these feedstocks varies significantly, requiring sophisticated process engineering. Safe control of high-temperature and high-pressure processes is required for the production of high-quality biofuel.

Storage and loading also present significant challenges. The tank farm must accurately record all inventories and correctly reflect storage and handling processes. It also needs to ensure transparent custody transfer subject to legal metrology for all material flows. The company’s goal was to realize a highly automated plant for continuous product and process monitoring even under variable raw material flows and complex process conditions.

Our solution: engineered instrumentation for reliable biodiesel production

From planning through to commissioning, TECOSOL GmbH, Endress+Hauser and the appointed project engineer worked in close partnership. Through intensive exchange and close coordination, the instrumentation was designed to meet the specific requirements of varying residues and waste materials, withstand high temperatures, pressures and vacuum conditions and be seamlessly integrated into the automation system.

Whether level, point level, flow, pressure or temperature, the complete product portfolio from Endress+Hauser covers all applications at the plant in Wittenberge, including analytical measurement technology and automation components.

문의처

저희 제품에 관심이 있으십니까? 해당 작업 용도에 대해 상담받고 싶은신가요?

문의 주시는 내용에 대해 최대한 상세하게 기재해 주시면, 보다 빠르고 정확한 응대가 가능합니다.

Products and services used

/

Related solutions and technology

온도 측정

오일 및 가스, 화학, 식음료, 생명 과학, 기초 원자재 및 금속, 발전 및 에너지 등 모든 프로세스 산업 유형에서 사용할 수 있는 가장 적합한 온도계를 선택하십시오.

추가 정보

소프트웨어 솔루션

엔드레스하우저는 모든 관련 측정 및 시스템 기술 외에도 운영 프로세스를 실행하는 모든 산업 분야에 적합한 소프트웨어를 제공합니다.

추가 정보

압력 측정

액체, 가스 및 증기의 압력 및 차압 측정

추가 정보

레벨 측정

액체 및 분체 레벨의 연속 및 포인트 측정이 가능한 엔드레스 하우저 레벨계 포트폴리오에서 가장 적합한 기기를 확인해 보십시오.

추가 정보

FAQs

Company logo of: S-IU - PSR - Template

TECOSOL GmbH는 유럽을 대표하는 바이오연료 생산업체 중 하나입니다. 독일 옥센푸르트에 본사를 두고 있으며, CO₂ 배출 저감 효과가 뛰어난 연료를 생산하고 있습니다. TECOSOL은 비텐베르게 사업장에 엔드레스하우저의 측정 기술을 전면 도입한 새로운 바이오디젤 플랜트를 구축하여 지속 가능한 생산과 순환 경제의 새로운 기준을 제시하고 있습니다.