High-quality instrumentation for cooling water systems
OEM Torishima benefits from reliable products and local service
Glasgow-based Torishima needs reliable and high-quality instrumentation for its cooling water systems which it supplies to municipal water customers in the Middle East. The company sources all of its instrumentation for the skids, including temperature transmitters, pressure transmitters and flowmeters, from Endress+Hauser and has praised the reliability and performance of the products, as well as the customer service.
The benefits
-
Remote access to instrumentation from the control room – essential in high-temperature environments.
-
Quality and durability of instrumentation.
-
On-time delivery.
-
Reliable and local customer service.
-
Expert support when needed.
The challenge
Cooling water systems are essential to ensure the safe, efficient and reliable operation of pumps and other equipment, as overheating can damage components, affect performance and compromise the overall stability and reliability of the pumping station. “These systems have to operate for 25 to 30 years, and breakdowns can be a major problem,” explains Projects and Operations Director Tom Coutts.
The solution
Endress+Hauser supplies temperature transmitters, pressure transmitters, point level switches, flowmeters and flow switches for the skids, all of which can be accessed remotely from the control room. In such demanding conditions, the quality and durability of the instrumentation is important. “Everything has to be stainless steel and to the strict specifications of the end user,” explains Tom. “If a cooling system goes down, it has a huge effect on the local community.”
Local support
On top of the need for high-performing equipment, good customer service is important to Torishima. “Some companies could be two or three months late with an order, but I’ve never had that problem with Endress+Hauser,” says Tom. “If I’ve got a problem I can pick up the phone and get the local agent to come in and discuss the situation. I prefer companies with a local presence, because it’s not always possible to explain the severity of a problem over the phone or by writing an email.”